Velocity_window_time

Index.Sub 606E.0H
Data Type Unsigned16
Access Read/Write
PDO Mappable No
Unit

milliseconds (ms)

Range

Unsigned16
Default Value 0
Store Supported No
Description This object is used to handle the bit10 (target reached) in the Statusword. When the difference between the Target_Velocity and the Velocity_Actual_Value is within the Velocity_window longer than the Velocity_window_time, the bit10 is set.

Notes

--